AXIS#.SAFEPARAM.ABSOLUTEPOSRESETSOURCE

Description

Indicates which inputs perform the safe homing. This is only configurable when the absolution position support is enabled (see AXIS#.SAFEPARAM.ABSOLUTEPOSEN) and a safe encoder is configured in the safety parameters.

Safe homing is required when AXIS#.SAFEPARAM.ABSOLUTEPOSVALID returns 0 (invalid). This means that a discrepancy between the position stored inside the SMM non-volatile memory and the absolute position returned by the safe encoder has been found.

Value

Description

0

Not Used

1

Safe Input 1 (SIN1)

2

Safe Input 2 (SIN2)

3

Safe Input 3 (SIN3)

4

Safe Input 4 (SIN4)

5

Safe dual Input 1 (SIN1/SIN2)

6

Safe dual Input 2 (SIN3/SIN4)

 

Parameters Editor with all of the Absolute Position Reset Source options showing and circled

Context

For safe encoder details refer to Motor feedback requirements.

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0, 1, 2, 3, 4, 5, 6

Default Value

0 (Not used)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.ABSOLUTEPOSRESETSOURCE

3150h

05h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.ABSOLUTEPOSRESETSOURCE

3250h

05h

Unsigned8

-

-

Read/Write

No